DOCA0098EN-11

Importing One or More Custom Models

You can import custom models.
  1. Click the Custom Library main tab.
  2. Click Import.

    The Import models dialog opens.

  3. Click Browse. The Open dialog appears.
  4. In the Opendialog, navigate to and select the custom model or models to import, then click Open.
  5. In the Import models dialog, click Import.
  6. After the import process is complete, click Close.

    The imported model or models appear in the Custom Library beneath the appropriate device type.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.