DOCA0098EN-11

Adding a Modbus Device Manually

Modbus devices that are not connected cannot be discovered, but they can be added manually using the following procedure.

You can add either a built-in Modbus device or a custom Modbus device that you have previously created in the Custom Library.

  1. Click the Device Settings main tab.
  2. Select the upstream device with a Modbus serial port in the device tree view.

    For example, the Com’X must be selected to connect a Modbus device to the Com’X.

  3. Select the Modbus Serial collapsible menu.Click the header to expand the Modbus Serial collapsible menu.
  4. Click Create a new device in the Device drop-down list.
  5. Select a Device Type in the drop-down list.
    NOTE: Only the devices that can be connected to a Modbus serial port are listed.
  6. Type the Slave ID in the Configuration collapsible menu.
  7. Click Create and the device appears in the device tree view.
** Refer to Common Properties for completing the other parameters.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.