DOCA0098EN-11

Deleting a Device

You can delete devices from the Com’X.
  1. Click the Device Settings main tab.
  2. Click the device to be deleted in the device tree view.
    NOTE: Do not deactivate the ZigBee network when removing ZigBee devices. Do not restart the Com’X until the Zigbee device has left the network. This can be confirmed by information in the maintenance log.
  3. Click Delete to confirm the deletion of the device.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.