DOCA0098EN-11

Disconnecting a Device

There is a procedure to disconnect a device from an upstream device.
When disconnected, the device does not appear in the Measurements Table. No measurement from this device is sent to the hosted platform. The device is still available in Real Time Data.
  1. Click the Device Settings main tab.
  2. Click the parent device in the device tree view.
  3. Select No device connected in the Connected to drop-down list.

    The device appears in the Devices not connected collapsible menu under the device tree view.

  4. Click Save changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.