DOCA0098EN-11

Reconnecting a Device

You can reconnect a device from an upstream device.
  1. Click the Device Settings main tab.
  2. In the device tree view, click the upstream device to which the downstream device must be connected.

    For example, select your Com’X to reconnect a downstream device to the Com’X.

  3. In the Digital and analog input collapsible menu, select the device to be reconnected on the required digital input.
  4. Click Save changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.