DOCA0098EN-11

Restoring the Configuration with a Local File

To restore configuration from a local file:

  1. Navigate to Maintenance > System Settings > Configuration Management.
  2. Click Browse in the Configuration Management collapsible menu to select the locally saved configuration file and click Open.
  3. Click Apply the configuration and wait for Com’X to reboot.

    The power LED turns green when the reboot is complete.

  4. Reconnect to the Com’X.
  5. If configuration files was saved using Backup for Duplicationthe following steps are required:
    1. Click Settings > Site Settings > Site Information.
    2. Type the new site location name, then click Save changes to save the modification.
      NOTE: The site location name may not include any of the following: '/:*?<>| or space.
    3. Click the Device Settings tab and select Com’X in the Device tree view and type the name in the General Propertiescollapsible menu.
    4. Click Save changes to save your modification.
  6. Click the Measurement table tab to check the correct connection, setting, and functioning on the new site.
  7. Select Commissioning tab to activate logging and publication according to destination platform.
    (see Commissioning for more information)
** (see Save the Configuration)
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.