DOCA0098EN-11

Restoring the Configuration with a USB Key

You can save configuration on a USB key and use it to restore configuration.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • This equipment must only be installed and serviced by qualified personnel.
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E in the USA, CSA Z462 or applicable local standards.
Failure to follow these instructions will result in death or serious injury.
  1. Copy the saved configuration file to a folder named "Restore" at the root of the USB key.
  2. Power off Com’X, then plug the USB key into the USB port on the Com’X front panel.
  3. Power on the Com’X and wait for it to reboot.

    When the power LED turns green, the reboot is complete.

  4. Log in to the Com’X.
  5. If configuration files was saved using Backup for Duplicationthe following steps are required:
    1. Click Settings > Site Settings > Site Information.
    2. Type the new site location name, then click Save changes to save the modification.
      NOTE: The site location name may not include any of the following: '/:*?<>| or space.
    3. Click the Device Settings tab and select Com’X in the Device tree view and type the name in the General Propertiescollapsible menu.
    4. Click Save changes to save your modification.
  6. Click the Measurement table tab to check the correct connection, setting, and functioning on the new site.
  7. Select Commissioning tab to activate logging and publication according to destination platform.
    (see Commissioning for more information)
** (see Save the Configuration
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.