DOCA0098EN-11

Upgrading Firmware via the USB Port

You can upgrade the firmware using the USB port.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • This equipment must only be installed and serviced by qualified personnel.
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E in the USA, CSA Z462 or applicable local standards.
Failure to follow these instructions will result in death or serious injury.
  1. Save the firmware file at the root of the USB memory key.
  2. Rename the file to upgrade.sp1.
  3. Make sure there is no file located at the root of the USB memory key with a name that is the same as the serial number of the Com’X.
  4. Power down the Com’X.
  5. Insert the USB memory key in the USB port located on the front face.
  6. Power up the Com’X.
  7. Wait up to 20 minutes for the Com’X to reboot.

    The power LED turns green when the reboot is complete.

  8. Connect to the Com’X through a PC and click the About link to check that the new firmware is installed.
  9. Clear browser cache after upgrade.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.