DOCA0098EN-11

Upgrading Firmware via the Web Page

You can upgrade the firmware through the web interface.
  1. Save the firmware file on your laptop.
  2. Click Maintenance > System settings.
  3. Click File in the Firmware upgrade collapsible menu, and select the firmware file.
  4. Click Open.

    The selected file appears in the field next to the Browse button.

  5. Click Upgrade Firmware.

    The message “Application not reachable” is displayed during the upgrade.

  6. Wait up to 20 minutes for the Com’X to reboot.

    The power LED turns green when the reboot is complete.

  7. Log in to the Com’X.
  8. Check that the new firmware has been installed in the About page.
  9. Clear browser cache after upgrade.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.