DOCA0098EN-11

Saving Real Time Trending Data Points or Graph

After the trending interval is complete or you have stopped sampling, you can export the data to a .csv file or save the graph as an image.
  1. Click EXPORT DATA, then follow your browser's prompts for saving the file. Alternatively, click VIEW POINTS, then click Export Data.
  2. To save the graph as an image, right-click the graph, then click Save image as. Follow your browser's prompts for saving the file.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.