DOCA0098EN-11

Using the Dashboard Kiosk

A user in a group with any modify permissions is subject to the Session Inactivity Timeout, configured in Group Settings.

To display a dashboard in kiosk mode with no session timeout, it is recommended to log in as a user in the default guest group. Alternatively, you can create a kiosk user group with view-only permissions for Dashboards and no other view or modify permissions.

To view the dashboard kiosk:

  1. View the dashboard.
  2. Click Kiosk.

    The dashboard opens in full screen mode.

NOTE: The graph updates only if the Period includes the current day. Otherwise, the dashboard remains static.
** (see Group Settings) as in Viewing a Dashboard
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.