DOCA0098EN-11

Viewing a Dashboard Graph or Table

You can view information dashboards.
  1. Click Monitoring > Dashboards.
  2. Click a dashboard category: Energy or Historical Trending.
  3. Select a device from Available Devices, then select a topic from Available Topics.
    NOTE: For Historical Trending, you can choose a single device with multiple topics (max 12) or multiple devices (max 4) with a single topic.
  4. Select the dashboard Period (Energy only).

    The requested graph displays.

  5. Optionally, you can refine the dashboard:
    1. Click the calendar icon to select a new start date for the Period.

      For Historical Trending, you can also select an end date to display up to 92 days.

    2. Select the type of graph.
    3. Click the divider between the device list and the graph to collapse the selection area and increase the dashboard's display area.
  6. Click VIEW POINTS to see the data in a table format.
    NOTE: The graph updates only if the Period includes the current day. Otherwise, the dashboard remains static.

    You can hover over a data point to view the value, date, and time. SeeUsing the Dashboard Kiosk for a full-screen dashboard view.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.