DOCA0098EN-11

Quickstart: Setting Up Publication

The steps below are a summary of publishing options. Refer to the appropriate sections for a full description of publishing per platform.
  1. Choose the platform and publication frequency as in Selecting Platform and Publication Frequency. For each platform, see these related tasks:
    • For a connection to a Schneider Electric subscribed service via Digital Service Platform (for example, EcoStruxure™ Facility Expert), see Connection.
    • For .csv export options, you may want to refer to File Format of CSV Export.
  2. Define the transfer protocol as in Define the Transfer Protocol
  3. Start the publication as in Starting the Publication
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.