DOCA0098EN-11

Quickstart: Setting Up and Starting Data Logging

Below are the general tasks related to starting data logging. There may be additional steps for publishing to a specific platform.
  1. Add the downstream devices as in Adding a Downstream Device. There are additional configuration tasks for each type of device:
    • Devices That Can Connect to Digital Inputs
      Should we create this topic so that the Device Settings map makes sense, or do separate links to the two topics: Built-in pulse meters(157353.xml), Custom pulse meters (157224.xml)
    • Devices That Can Connect to Analog Inputs
      Same as above, there are two topics: Resistance temp detectors (157324.xml), custom analog devices (157226.xml)
    • Modbus Devices
      Same as above, there are three topics: Discovering connected devices (157294.xml), Adding Modbus device manually (157176.xml), Connecting devices to Acti9 (157178.xml)
    • Ethernet Device Configuration Parameters
  2. Select the measurements to log as in Selecting Measurements to Log or Publish
  3. Define the logging intervals as in Defining the Logging Intervals
  4. Start the data logging as in Starting the Data Logging.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.