DOCA0098EN-11

Quickstart: Viewing On-board Data

You can view real time and logged data on the Com’X 510 without having to connect to a hosted platform. Below are the steps for viewing on-board data.
  1. Add the downstream devices as in Adding a Downstream Device. There are additional configuration tasks for each type of device:
    • Modbus Devices
      Same as above, there are three topics: Discovering connected devices (157294.xml), Adding Modbus device manually (157176.xml), Connecting devices to Acti9 (157178.xml)
    • Ethernet Device Configuration Parameters
  2. Complete the following steps to view an Energy dashboard or Historical Trending. Skip to step 3 to view real time data.
    1. Selecting Measurements to Log or Publish
    2. Defining the Logging Intervals
    3. Starting the Data Logging.
    NOTE: The amount of data collected affects the ability to display certain dashboard options, for example a year over year dashboard.
  3. View real time data for one or more devices: Viewing Real Time Data for a Single Device or Viewing a Device Summary.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.