DOCA0098EN-11

Resetting Device Parameters

You can reset device parameters.
  1. Click Control > Resets > Device Resets.
  2. Select the devices you want to reset from the Device Selection list.
  3. Select the reset operation from Reset Options.
  4. Enter the password for each device requiring a password.
    NOTE: The default password check box is populated by the default password provided by the device and is selected by default. You can deselect the default password check box and enter another password.
    The Resets button becomes available.
  5. Click Reset.

    The selected device parameters are reset and the status displays as "ok."

NOTE: Date/Time values are reported only when the device supports them. For example, if a device does not support the Min/Max value for "Date/Time Last Reset," the "Min/Max" value will not be populated here.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.