DOCA0098EN-11

Running Network Diagnostics

You can run diagnostic tests for the network and server connections.
  1. Navigate toSettings > General Settings > Network Settings.
  2. Click Launch diagnostic in the Diagnostic network menu.
    A new Diagnostic Network window opens which shows the progress and status of the diagnostic tests.
  3. Click Start to restart the network diagnostics or click Close to exit the Diagnostic Network window.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.