DOCA0098EN-11

Configuring Links

You can add links to the Com’X.
  1. Click Settings > Links > Setup Links.

    The Links page opens.

  2. Enter a name and description for the link.
  3. Enter a number 1 to 100 in the Priority field.
    NOTE: Negative priority is reserved for built-in links. Links display in ascending order of priority.
  4. Click the type of link, then:
    1. For Link to File, browse to select the file.
      NOTE: Only PDF files can be uploaded. An error message displays when you try to upload any other file type.
    2. For Link to URL, enter the URL
  5. Click Add. The link is added to the setup list and View Links 

You can change the type of link after it has been created. To edit a link, click Edit, make the desired changes, then click Update.

To delete a link, click the check box beside the link name, then click Remove.

**(see Viewing Links)
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.