DOCA0098EN-11

Adding a Custom Web Page

The init.js file is required for each web page.

Any file referenced by init.js is also required for the page to be valid and viewable.

Before uploading any files, compare the size of the custom page file set with the Available Storage.

NOTE: Allowed file types are html, shtml, htm, js, jpg, jpeg, png, gif, and css. An error message displays when you try to upload any other file type.

NOTICE
IMPAIRED COM'X PERFORMANCE
Do not add more than 10 MB of files to Custom Page Management.
Failure to follow these instructions can impair Com'X performance.

To view the newly added web page, you must log out and log in again.

  1. Click Settings > Custom Page Management.
  2. Click Create, then enter the name you want to display on the web page.
  3. Click OK. The web page container displays in the list of custom web pages with a validation error.
  4. Click Edit to add the web page files.
  5. Click Upload, then select the custom page files from your computer.
  6. Click OK. The Com’X validates that files called by init.js are present.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.