DOCA0098EN-11

Configuring Date and Time

The time and date settings must be set to the current date and time before enabling Schneider Electric Services on your Com’X.

Any manual changes on the date and time are overwritten by Digital Service Platform. You can only edit the Timezone.

It is recommended that DST time zone is selected when using Energy Operation to ensure consistent time stamping with the Com’X.

To set the date and time:

  1. Click Settings > General Settings > Date/Time Settings.
  2. Select the appropriate Timezone in the drop-down list. If a DST time zone is selected, the clock will automatically adjust for Daylight Saving Time.
  3. Choose one of the following:
    1. Click the Today button to set the date and time automatically with the date and time of your computer.
    2. Manually enter the date and time in the date and time fields.
    3. Select Yes for SNTP support, then enter an SNTP server address. (Default: pool.ntp.org)
  4. Click Save changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.