DOCA0098EN-11

Configuring FTP Transfer Protocol

You can configure FTP as the file transfer protocol for publications.
NOTE: FTP is not a secure protocol, as login IDs and passwords are communicated in plain text. Schneider Electric strongly recommends using only HTTPS protocol for security purposes. Refer to Security Configuration Recommendations for additional information regarding risks associated with unsecure protocols and recommended best practices.
  1. Click Settings > General Settings > Publication.
  2. Select the Destination platform in the drop-down list.
  3. Select FTP in the Protocol drop-down list.
  4. Type the address of the server transporting the data in the Server field.

    Server address for Energy Operation is automatically filled. Do not modify the server address.

  5. Type the outgoing delivery port in the Port field.

    The factory setting is 21.

  6. Select Yes in the Authentication required field for any platform requiring authentication, for example Energy Operation.
  7. Type the username and the password.

    For Schneider Electric platforms, this information is given with the subscription contract. Contact the Schneider Electric representative to provide you with this information.

  8. For CSV, type the directory information for the remote server in the Directory field.
  9. Click Save changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.