DOCA0098EN-11

Configuring Firewall Settings

You can configure firewall settings.

NOTE: HTTP and Modbus are not a secure protocols. Schneider Electric strongly recommends using only HTTPS protocol. Disable the HTTP and Modbus ports for each interface for security purposes. If Modbus access is required, Schneider Electric strongly recommends using Modbus IP filtering feature for added security.

  1. Click Settings > Security > Firewall Management. Configure each interface by protocol according to the available options above.
    NOTE: Editable port numbers can be set to the default value or any port number above 1023.
  2. Alternatively, click Defaults to reset to defaults.
  3. Click Save changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.