DOCA0098EN-11

Configuring a Wi-Fi Network

You can configure your Com’X wireless network.
  1. Click Settings > General Settings > Network Settings.
  2. Select WiFi only or WiFi and 2 Switched Ports (1 IP address network) in the Choose your network configuration dropdown list.
    NOTE: Schneider Electric recommends using WPA2.
  3. Click Select a Wi-Fi network in the Wi-Fi settings collapsible menu.
  4. Click Refresh network list to scan all the Wi-Fi networks available.
  5. Select the Wi-Fi network required. Type the key in the Secure key field if the key does not appear automatically.
  6. Select Other if the required Wi-Fi network does not automatically appear in the list of Wi-Fi networks. Type the SSID and the key in the Secure key field.
  7. Click Save changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.