DOCA0098EN-11

Copying an Event

You can create a new event from an existing event.
  1. Click Settings > Events > Custom Events.
  2. Click the existing event name.
  3. Click on the green event block in the workspace, then press CTRL+C.
  4. Click Cancel to return to the Custom Event Library.
  5. Click New Custom Event.
  6. Click inside the workspace, then press CRTL+V.

    The event block is pasted into the workspace.

  7. Edit the device, topic, or values, then click Save changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.