DOCA0098EN-11

Defining the Logging Intervals

It is important to consider how much data is being logged across all devices when selecting the logging interval and number of topics to log.

Logging too many topics per interval may affect Com’X performance, including degraded web page response and missed logging intervals.

For example, for a logging interval of less than five minutes, it is recommended that you log no more than 8 devices with 50 total topics.

  1. Click Settings > Site Settings > Data Logging.
  2. Select your country.
    NOTE: This will automatically set the logging intervals of data for different commodities in the country. You can also edit these intervals individually.
  3. Click Save changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.