DOCA0098EN-11

Editing or Deleting a Custom Event

**
You can modify or remove events from the Custom Event Library.
  1. Click Settings > Events > Custom Events.
  2. Click the event name.
  3. Either edit the event block and click Save changes, or click Delete to remove the event from the Custom Event Library.
    Refer to Troubleshooting if you do not receive the event through the selected Action.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.