DOCA0098EN-11

Modifying a User

You can modify user settings except for the username and password.

An administrator cannot modify the username or password after the user is created. If you forget your username or password, contact an administrator to delete the account and create a new one.

  1. Click Settings > User Management > Users.
  2. Select the user you want to modify.
  3. Modify the fields you want to change, then click Save changes.

The user must change the password after logging in for the first time.

** See Changing the Password
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.