DOCA0098EN-11

Selecting Platform and Publication Frequency

Use the Publication subtab to select the platform to which the logged data is sent and at what frequency.
  1. Click Settings > General Settings > Publication.
  2. Select the Destination platform in the drop-down list.
  3. Select how often the data is sent in the Publication frequency drop-down list:
    • Weekly: select the day of the week.
    • Daily: the data is sent at 1:00 a.m. local time.
    • For higher frequencies, publication times are calculated starting at 0:00 a.m. For example, if Every 2 hours is selected, data is sent at 0:00 a.m., 2:00 a.m., 4:00 a.m., and so on. If Every 3 hours is selected, data is sent at 0:00 a.m., 3:00 a.m., 6:00 a.m., and so on.
  4. Click Save changes.

    The first publication occurs on the first hour that matches the selected frequency after the Start publication task. For example, if Every 2 hours is selected and the publication starts at 9:45 a.m., the first publication is at 10:00 a.m.

    see Commissioning.
NOTE: DSP will be available as a drop-down option under Destination platform only after you enable Schneider Electric services.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.