DOCA0098EN-11

Uploading a New Certificate

You can install a new HTTPS certificate on your device.

It is recommended to create a backup of your configuration before installing a new certificate. To update the HTTPS certificate:

  1. Click Settings > Security > Certificates.
  2. Click inside the text box Install a new certificate.
  3. In the browser, select your *.pem file, then click Open.
  4. Click Install. The Installed certificate details update to display the new certificate.

To remove the current certificate and set the Com’X back to the factory default certificate, click Reset.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.