DOCA0098EN-11

Setting Time on Devices

The Localized Time is the current date and time on the selected device, adjusted to reflect the time zone selected in the Com’X Date/Time Settings.
  1. Click Control > Set Device Time.
  2. Select the devices you want to reset from the Device Selection list.
  3. Click Get Time to display the Localized Time for the device.
  4. Click Set Time to send the Com’X date/time (UTC) to the device. The status displays as either Successful or Unsuccessful.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.