DOCA0036EN-14

Remote Access with Windows Operating Systems

You can remotely access the Com’X by using an IP address under Windows XP.

The IT administrator should be requested to provide a fixed IP address to assign systematically the same IP address to the Com’X.

With Windows, the Com’X is accessible under Windows Explorer when connecting the PC to the same LAN. It is not necessary to know the IP address.

** (see With Windows 7/Vista)
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.