DOCA0036EN-14

Static IP Settings

In the Com’X, you can define the IPv4 addresses of the Ethernet interface, subnetwork mask, and default gateway.

These settings must be consistent with the network policy of the site. The IT administrator of the site should be contacted to provide this information.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.