DOCA0036EN-14

Network Settings

Change title?
The Com’X offers several connection interfaces.

  • Ethernet with two ports
  • Wi-Fi
  • GPRS or 3G for isolated sites or sites where the IT administrator does not allow access to the network infrastructure.

The available interfaces are determined by the accessories connected to the Com’X: GPRS or 3G modem or Wi-Fi USB key.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.