DOCA0036EN-14

DHCP Server Over Wi-Fi

When a Wi-Fi key is connected to the Com’X, you can configure the Com’X so that it creates a Wi-Fi access point.

In that case, the Com’X creates a Wi-Fi network with an SSID using the same name as the Com’X but without any access restriction (no WEP nor WPA authentication) in this mode. The Com’X configures its Wi-Fi interface with the IP address 10.25.2.1.

The Com’X also starts an internal DHCP server on this Wi-Fi interface. It enables you to assign automatically an IP address, consistent with its own address, to any Wi-Fi devices that are configured to operate as DHCP clients.

IP addresses assigned by the Com’X are in the subnetwork 10.25.2.0/24 (starting from 10.25.2.65, 10.25.2.66, and so on). The Com’X has no routing capabilities. As a result, no Default Gateway nor Domain Name Server are sent by this DHCP server.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.