DOCA0036EN-14

IPv4 Address Settings

The Com’X supports three different operating modes for assigning the IP address.

These modes are:

  • Static IPv4
  • DHCP client
  • DHCP server

** (see Static IP Settings)(see DHCP Client)(seeDHCP Server Over Ethernet Port or DHCP Server Over Wi-Fi)
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.