DOCA0036EN-14

ZigBee Network Settings

You can add up to 20 ZigBee devices to the Com’X (Zigbee dongle EBXA-USB-Zigbee defines the number of ZigBee devices allowed).

ZigBee is a wireless networking standard for remote control and sensor applications.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.