DOCA0036EN-14

Custom Main Meter

After you create a custom main meter model in the Custom Library, you can add instances of that custom main meter in the Device Settings.

When you add a custom main meter, the two pulse outputs are automatically connected to the upstream device. You can connect the four contact outputs as in Connecting a Standard Main Meter

**see Connecting a Standard Main Meter
.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.