DOCA0036EN-14

Custom Analog Sensor Model

**
Each custom analog sensor model monitors a single point.

The Com’X offers two analog sensor templates:

  • 4...20 mA
  • 0...10 V

You can create a customized analog sensor model by entering customized settings for the following properties:

  • Count element
  • Count unit

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.