DOCA0036EN-14

Custom Modbus Devices

The Com’X can also communicate with any third-party Modbus device. This type of Modbus device is called Modbus serial line custom slave.

The Com’X is able to communicate with a Modbus serial line custom slave in two ways:

  • directly by using its own serial port
  • through a ModbusTCP/Modbus serial line gateway

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.