DOCA0036EN-14

Built-in Ethernet Devices

You can add built-in Ethernet devices to your system.

In the system, you can add these devices:

  • Modbus TCP/IP to Modbus serial line gateways. These gateways are used to collect data from serial devices.
  • Modbus TCP/IP meters.
  • Custom Modbus TCP/IP to serial gateway used to collect data from serial devices.

NOTE: To collect data from a PM800 series meter with an Ethernet card and use this PM800 as a gateway, you must define 2 devices: the meter (for example, PM850ECC) and the gateway (PM8ECC Modbus gateway).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.