DOCA0036EN-14

Custom Analog Devices

You can add an analog device that is based on a custom analog device model.

Before adding a custom device you first need to create the custom model in the Custom Library.

** (Custom Models)
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.