DOCA0036EN-14

Modbus Meter Measurements

The Com’X retrieves available measurements from Schneider Electric Modbus meters.

Available measurements include:

  • total active energy
  • active energy per phase
  • total reactive energy
  • reactive energy per phase
  • total apparent energy
  • active power
  • reactive power
  • apparent power
  • phase-neutral voltages
  • phase-phase voltages
  • phase and neutral currents
  • frequency
  • power factor
  • total harmonic distortion

Additional Measurements for Built-in Devices

For additional measurements, you must create a new model of the device based on an existing built-in device, and then customize it to your needs. Refer to the data sheet of the specific meter to identify which Modbus registers correspond to the measurement required.

(see Creating a Custom Model)Refer to Replacing a Device for instructions on how to replace a built-in device with a custom device.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.