DOCA0036EN-14

Main Features

The Com’X 210 has several main features.

  • Automatic discovery of connected Modbus devices
  • Connectivity to the cloud through three media: Cellular, wired Ethernet, or Wi-Fi Ethernet
  • Two Ethernet ports to separate upstream cloud connection from field device network
  • Four supported transfer protocols: HTTP, HTTPS, FTP, and SMTP with proxy management
  • Data storage in case of upstream communication interruption
  • Data export with native connection to Schneider Electric service platforms (such as Energy Operation) and with .csv file for other database servers
  • Gateway functionality Modbus TCP to Modbus RTU
  • Setup through on-board web pages
  • Compliant with electrical switchboard environment (temperature, electromagnetic compatibility)
  • Local backup of configuration parameters
  • ZigBee Pro with EM4300 sensors

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.