DOCA0036EN-14

Product Overview

The Com’X 210 energy server is a compact plug and play data logger.

The Com’X 210 collects and stores consumption of WAGES (Water, Air, Gas, Electricity, and Steam) and environmental parameters such as temperature, humidity, and CO2 levels in a building. Data can be securely transmitted as a report to an Internet database server.

Data is ready to be processed once received by the server. Data is displayed as web pages through energy management services provided by Schneider Electric, such as EcoStruxure™Energy Operation and EcoStruxure™ Facility Expert, to support optimization of energy performance and cost management.

The Com’X 210 also provides a transparent interface between Ethernet-based networks and field devices. This gateway function supports the use of monitoring software to access information from devices for data collection, trending, event management, analysis, and other functions.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?