DOCA0036EN-14

Upgrade Firmware

The Com’X can be updated using secured firmware through the web page or the USB port on the Com’X front face.

For the latest firmware update, check www.se.com on the Com’X page, or contact your local sales representative.

Firmware upgrades can only be successful if the date and time of the Com’X is correctly configured.

**

Before You Begin

  • You should save a backup configuration before and after each firmware upgrade.
    **
  • Manually push any logged data in Commissioning > Publication > Manual publication.
NOTE: Depending on the number of devices connected to the Com’X, it can take 10 to 35 minutes to upgrade the firmware and reboot the Com’X.
** (see Configuring Date and Time) (see Save the Configuration)
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.