DOCA0036EN-14

Data Logging

The Com’X can log data at pre-defined intervals.

The logging interval can be set for each type of commodity, for example, electricity, water, or gas. Each device can report only one type of commodity.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.