DOCA0036EN-14

Email Settings

Email Settings allows you to configure the connection to an SMTP server to publish a .csv file over SMTP.
NOTICE
DATA PRIVACY INFRINGEMENT
Comply with regional data privacy regulations and laws when using individual email addresses and personal information.
Failure to follow these instructions can result in complaints, liability, or penalties for non-compliance with applicable data protection regulations.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.