DOCA0036EN-14

Warning Banner Overview

The Warning Banner allows you to display a message to warn against unauthorized use and advice authorized users of their obligations relating to acceptable use of the Com’X. This feature is disabled by default. Once enabled, a user can access Com’X login page only after agreeing to the terms and conditions displayed in the Warning Banner.

You can configure the following:

  • Enable warning banner – allows you to enable the warning banner to be displayed for users prior to login. This is disabled by default. Once enabled, the warning banner text field displays.

  • Warning banner text –You can enter desired text to warn against unauthorized use and notify authorized users of their obligations relating to acceptable use of Com’X. A maximum of 4000 characters is allowed. If you enter more than 4000 characters, the text displays in red and the Save changes button is disabled.

  • Defaults – allows you revert to default settings. The Warning Banner gets disabled and the Warning banner text field is hidden.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.