DOCA0036EN-14

Supported Web Browsers

You can access the energy server using a variety of web browsers.
Browser Browser Version
Microsoft Edge 42.0 and above
Internet Explorer IE9 and above
Firefox 20.0 and above
Chrome 24.0 and above

Recommended Web Browsers

It is recommended to use Chrome for PC.

The following browsers are recommended for tablets:

Operating System Browser
Windows 10
  • Microsoft Edge
Windows 8
  • Internet Explorer
  • Firefox
iOS
  • Chrome
  • Safari
Android
  • Chrome
  • Android browser

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.