DOCA0036EN-14

Advanced Ethernet Settings

Advanced Ethernet Settings allow you to customize network settings for your specific environment.

The defined parameters apply to both Ethernet ports.

Setting Description Options
Time to Live Identifies the number of routers a TCP packet can pass before it is discarded.

1-255 hops

Default: 60 hops

Enable TCP Keep Alive A keepalive is a message sent to check that the link between the Com’X and its connected host is operating, or to prevent this link from being broken.

Yes or No

Default: Yes

Time Elapsed time between two successive keepalive retransmissions, if acknowledgment to the previous transmission is not received.

1-7200 seconds

Default: 30 seconds

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.